1.2.1.22.2 Trivial File Transfer Protocol (TFTP) Client Configurations
TFTP Client Specific User Configurations
TFTP Client Maximum Retries:
The number of attempts before declaring a TIMEOUT error.
Default value: 3
Symbol TCPIP_TFTPC_MAX_RETRIES
Maximum Length for File name:
The maximum value for the file name size.
Default value: 32
Symbol TCPIP_TFTPC_FILENAME_LEN
Enable Console Commands:
Enable the TFTP TCP/IP Console Commands
Default value: false
Symbol: TCPIP_TFTPC_CONSOLE_CMD
TFTP Task Rate (in msec):
TFTP task processing rate, in milliseconds.
The TFTP module will process a timer event with this rate for maintaining its own queues, processing timeouts, etc.
The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained
The value cannot be lower than the TCPIP_STACK_TICK_RATE.
Default value: 100
Symbol TCPIP_TFTPC_TASK_TICK_RATE
Enable User Notification:
Allow TFTP client user notification
If enabled, the TCPIP_TFTPC_HandlerRegister/TCPIP_TFTPC_HandlerDeRegister functions exist and can be used
Default value: false
Symbol TCPIP_TFTPC_USER_NOTIFICATION
Maximum Length for Server Address:
The maximum length to store the server address
Default value: 40
Symbol TCPIP_TFTPC_SERVERADDRESS_LEN
TFTP Client Socket Connection Timeout (in sec):
The number of seconds to wait before declaring a TIMEOUT error on PUT.
Value is in seconds
Default value: 3
Symbol TCPIP_TFTPC_ARP_TIMEOUT
TFTP Client Command Process Timeout (in sec):
The number of seconds to wait before declaring a TIMEOUT error on GET.
Value is in seconds
Default value: 3
Symbol TCPIP_TFTPC_CMD_PROCESS_TIMEOUT
Default Interface:
The default TFTP interface for multi-homed hosts.
Default value: interface 0
Symbol TCPIP_TFTPC_DEFAULT_IF