1.2.1.8.2 Domain Name System Server (DNSS) Configurations
DNSS Specific User Configurations
Maximum Number of IPv4 Cache Entries:
Maximum and default number of IPv4 entries will be allowed to be configured from command prompt.
These many entries will be allowed to be sent in response for the DNS query with record type TCPIP_DNS_TYPE_A.
Default value: 2
Symbol TCPIP_DNSS_CACHE_PER_IPV4_ADDRESS
Maximum Number of IPv6 Cache Entries:
Maximum and default number of IPv6 entries will be allowed to be configured from command prompt.
Tthese many entries will be allowed to be sent in response for the DNS query with record type TCPIP_DNS_TYPE_AAAA.
Default value: 1
Symbol TCPIP_DNSS_CACHE_PER_IPV6_ADDRESS
Default DNS Host Name Length:
Default DNS host name length
Default value: 64
Symbol TCPIP_DNSS_HOST_NAME_LEN
Enable Console Commands:
Enable the DNSS TCP/IP Console Commands
Default value: false
Symbol: TCPIP_DNSS_CONSOLE_CMD
DNS Server Task Rate (in msec):
DNSS task processing rate, in milliseconds.
The DNSS module will process a timer event with this rate for maintaining its own queues, processing timeouts, etc.
The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained
The value cannot be lower than the TCPIP_STACK_TICK_RATE.
Default value: 33
Symbol TCPIP_DNSS_TASK_PROCESS_RATE
Default DNS Server Time-To-Live(in sec):
Default TTL time for a IP address
Value is in seconds
Default value: (10 * 60)
Symbol TCPIP_DNSS_TTL_TIME
Delete Old Cache if Still in Place:
On initialization, delete the old cache if still in place
Else do not re-initialize
Default value: true
Symbol TCPIP_DNSS_DELETE_OLD_LEASE
Reply to Client Request with Board Info:
Reply DNS info with Board info only if the requested DNS host name is not present
if TCPIP_DNSS_REPLY_BOARD_ADDR != true, then return no such name
Default value: true
Symbol TCPIP_DNSS_REPLY_BOARD_ADDR