1.2.1.3.2 Dynamic Host Configuration Protocol (DCHP) Configurations
DCHP Client Specific User Configurations
DHCP Request Time-out (in sec):
Defines how long to wait before a DHCP lease is acquired when the DHCP module is enabled
Value is in seconds
Default value: 10
Symbol TCPIP_DHCP_TIMEOUT
DHCP Host Name Maximum Size:
Maximum size of a host name to be advertised to the DHCP server
Default value: 20
Symbol TCPIP_DHCP_HOST_NAME_SIZE
Enable Console Commands:
Enable the DHCP TCP/IP Console Commands
Default value: false
Symbol: TCPIP_DHCP_CLIENT_CONSOLE_CMD
DHCP Client Task Rate (in msec):
The DHCP task processing rate: number of milliseconds to generate an DHCP tick.
Used by the DHCP state machine
The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained
The value cannot be lower than the TCPIP_STACK_TICK_RATE.
Default value: 200
Symbol TCPIP_DHCP_TASK_TICK_RATE
Client Port for DHCP Client Transactions:
Local UDP port number for the DHCP Client Transactions
Default value: 68
Symbol TCPIP_DHCP_CLIENT_CONNECT_PORT
Remote Server Port for DHCP Server Messages:
Remote UDP port number for the DHCP Client Transactions
Default value: 67
Symbol TCPIP_DHCP_SERVER_LISTEN_PORT
Enable the time server option:
Enables the request of the time server option
Default value: 0
Symbol TCPIP_DHCP_USE_OPTION_TIME_SERVER
Maximum Number of Time Servers to Store:
Max number of time server addresses to store
Should be less than 256!
Only if TCPIP_DHCP_USE_OPTION_TIME_SERVER is enabled
Default value: 1
Symbol TCPIP_DHCP_TIME_SERVER_ADDRESSES, TCPIP_DHCP_OPTION_TIME_SERVER_MAX
Enable the NTP server option:
Enables the request of the NTP server option
Default value: 0
Symbol TCPIP_DHCP_USE_OPTION_NTP_SERVER
Maximum Number of NTP Servers to Store:
Max number of NTP server addresses to store
Should be less than 256!
Only if TCPIP_DHCP_USE_OPTION_NTP_SERVER is enabled
Default value: 1
Symbol TCPIP_DHCP_NTP_SERVER_ADDRESSES, TCPIP_DHCP_OPTION_NTP_SERVER_MAX
Enable the DHCP client:
Default value for the enable/disable the DHCP client at stack start-up.
Note: the interface initialization setting in TCPIP_NETWORK_CONFIG takes precedence!
Default value: none
Symbol TCPIP_DHCP_CLIENT_ENABLED
Boot File Name Option:
Enable the usage of the Boot file name received from the DHCP server
Default value: false
Symbol TCPIP_DHCP_STORE_BOOT_FILE_NAME
Boot file name storage size:
Size of the storage for the Boot file name
should always be <= 128
Default value: 128
Symbol TCPIP_DHCP_BOOT_FILE_NAME_SIZE