TCPIP_SMTPC_MESSAGE_WARNING Enumeration

C

typedef enum {
TCPIP_SMTPC_WARN_REPLY_BUFFER_SMALL = 0x0001,
TCPIP_SMTPC_WARN_WRONG_FORMAT = 0x0002,
TCPIP_SMTPC_WARN_UNEXPECTED_REPLY = 0x0004,
TCPIP_SMTPC_WARN_FILE_NOT_FOUND = 0x0008,
TCPIP_SMTPC_WARN_AUTH_LOGIN_LEN = 0x0010
} TCPIP_SMTPC_MESSAGE_WARNING;

Description

Enumeration: TCPIP_SMTPC_MESSAGE_WARNING.

Enumeration describing the possible warning types occurring during a mail transmission. These events are not fatal and SMTPC client will try to complete the mail transfer.

Parameters

ParametersDescription
TCPIP_SMTPC_WARN_REPLY_BUFFER_SMALL = 0x0001The reply buffer allocated for the server replies is too small server reply exceeded the size of the buffer it should be increased.
TCPIP_SMTPC_WARN_WRONG_FORMAT = 0x0002Server reply was not properly formatted.
TCPIP_SMTPC_WARN_UNEXPECTED_REPLY = 0x0004Unexpected server replied received.
TCPIP_SMTPC_WARN_FILE_NOT_FOUND = 0x0008File attachment not found; ignored.
TCPIP_SMTPC_WARN_AUTH_LOGIN_LEN = 0x0010Provided credentials for LOGIN authentication are too long and were truncated (buffer overflow) this most likely will result in a server authentication rejection.

Remarks

Multiple warnings could be set during a mail transmission.