TCPIP_TFTPC_OPERATION_RESULT Enumeration
C
typedef enum {
TFTPC_ERROR_NONE = 0,
TFTPC_ERROR_FILE_NOT_FOUND = -1,
TFTPC_ERROR_BUSY = -2,
TFTPC_ERROR_DISK_FULL = -3,
TFTPC_ERROR_INVALID_OPERATION = -4,
TFTPC_ERROR_UNKNOWN_TID = -5,
TFTPC_ERROR_FILE_EXISTS = -6,
TFTPC_ERROR_NO_SUCH_USE = -7,
TFTPC_ERROR_DNS_RESOLVE_ERR = -8,
TFTPC_ERROR_INVALID_INTERFACE = -9,
TFTPC_ERROR_INVALID_FILE_LENGTH = -10,
TFTPC_ERROR_INVALID_SERVER_ADDR = -11
} TCPIP_TFTPC_OPERATION_RESULT;
Description
Enumeration: TCPIP_TFTPC_OPERATION_RESULT.
This enumeration defines the standard error codes for TFTP PUT and GET command operation.
Members
Members | Description |
---|---|
TFTPC_ERROR_FILE_NOT_FOUND = -1 | TFTP client file not found. |
TFTPC_ERROR_BUSY = -2 | TFTP client is busy when one file PUT or GET transfer is going on. |
TFTPC_ERROR_DISK_FULL = -3 | TFTP client buffer full. |
TFTPC_ERROR_INVALID_OPERATION = -4 | TFTP client invalid command operation. |
TFTPC_ERROR_UNKNOWN_TID = -5 | TfTP ID error. |
TFTPC_ERROR_FILE_EXISTS = -6 | TFTP client file already exists. |
TFTPC_ERROR_NO_SUCH_USE = -7 | TFTP client not in use. |
TFTPC_ERROR_DNS_RESOLVE_ERR = -8 | TFTP client DNS resolve error. |
TFTPC_ERROR_INVALID_INTERFACE = -9 | TFTP client interface error. |
TFTPC_ERROR_INVALID_FILE_LENGTH = -10 | TFTP client file length is more than the expected size, which should be the size of SYS_FS_FILE_NAME_LEN. |
TFTPC_ERROR_INVALID_SERVER_ADDR = -11 | Invali Server Address. |