TCPIP_TFTPC_SetServerAddress Function
C
void TCPIP_TFTPC_SetServerAddress(
IP_MULTI_ADDRESS* ipAddr,
IP_ADDRESS_TYPE ipType
);
Description
This function is used to set the TFTP server address (either it will be IPv4 address or IPv5 address). This address will be used for either GET or PUT mode of TFTP client operation.
Preconditions
The TFTP client module must be initialized.
Parameters
Parameters | Description |
---|---|
ipAddr | Pointer to the server address. |
ipType | Type of address: IPv4/IPv6. |
Returns
None.
Remarks
None.