TCPIP_ARP_EntryQuery Function
C
TCPIP_ARP_RESULT TCPIP_ARP_EntryQuery(
TCPIP_NET_HANDLE hNet,
size_t index,
TCPIP_ARP_ENTRY_QUERY* pArpQuery
);
Description
This function can be used for displaying the cache contents.
Preconditions
The ARP module should have been initialized. The index has to be a valid one. For example, TCPIP_ARP_CacheEntriesNoGet populates the supplied TCPIP_ARP_ENTRY_QUERY query entry.
Parameters
Parameters | Description |
---|---|
hNet | Interface handle to use. |
index | Index to cache. |
pArpQuery | Entry type, IP address, hardware address. |
Returns
On Success - ARP_RES_OK.
On Failure - ARP_RES_BAD_INDEX (if index is out of range) ARP_RES_NO_INTERFACE (if no such interface exists) .
Remarks
None.