TCPIP_TELNET_AuthenticationDeregister Function
C
bool TCPIP_TELNET_AuthenticationDeregister(
TCPIP_TELNET_HANDLE authHandle
);
Description
This function removes a authentication handler.
Preconditions
Telnet properly initialized.
Parameters
Parameters | Description |
---|---|
authHandler | TCPIP_TELNET_HANDLE obtained by a call to TCPIP_TELNET_AuthenticationRegister(). |
Returns
True - If the operation succeeded.
False - If the operation failed.
Remarks
The build should have TCPIP_TELNET_OBSOLETE_AUTHENTICATION == false.
Example
TCPIP_TELNET_HANDLE myHandle = TCPIP_TELNET_AuthenticationRegister(myAuthHandler, myParam );
// process incoming login requests
// now we're done with it
// no more users will be able to login
TCPIP_TELNET_AuthenticationDeregister(myHandle);