10.1.2 Return Address Stack
The return address stack allows any combination of up to 31 program
calls and interrupts to occur. The PC is pushed onto the stack when a CALL
or RCALL
instruction is executed or an interrupt is Acknowledged. The PC
value is pulled off the stack on a RETURN
, RETLW
or a
RETFIE
instruction. PCLATU and PCLATH are not affected by any of the
RETURN
or CALL
instructions.
The stack operates as a 31-word by 21-bit RAM and a 5-bit Stack Pointer, or as a 35-word by 21-bit RAM with a 6-bit Stack Pointer in ICD mode. The stack space is not part of either program or data space. The Stack Pointer is readable and writable and the address on the top of the stack is readable and writable through the Top-of-Stack (TOS) Special File registers. Data can also be pushed to, or popped from the stack, using these registers.
A CALL
type instruction causes a push onto the
stack; the Stack Pointer is first incremented and the location pointed to by the Stack
Pointer is written with the contents of the PC (already pointing to the instruction
following the CALL
). A RETURN
type
instruction causes a pop from the stack; the contents of the location pointed to by the
STKPTR are transferred to the PC and then the Stack Pointer is decremented.
The Stack Pointer is initialized to ‘0b00000’ after all Resets. There is no RAM associated with the location corresponding to a Stack Pointer value of ‘0b00000’; this is only a Reset value. Status bits in the PCON0 register indicate if the stack is full or has overflowed or has under-flowed.