5.6.2.6 .porg new-lc[, fill]
Advance the location counter of the current section to
new-lc. In program
memory,new-lc is specified in PC units. On the
dsPIC33C/E/F device, the PC increments by 2 for each instruction word. Odd values are not
permitted. On a dsPIC33A device, the PC increments by 4 for each instruction word.
.porg occurs.The bytes between the current location counter and the new location
counter are filled with fill.
new-lc is an absolute expression. You cannot
.porg backwards. You cannot use .porg to cross
sections.
The new location counter is relative to the current module and is not an absolute address.
This directive is only allowed in a code section. If not in a code section, a warning is generated and the rest of the line is ignored.
fill is optional. If not specified, it
defaults to the last .pfillvalue specified.