5.6.2.5 .org new-lc[, fill]
Advance the location counter of the current section to
new-lc. In program
memory,new-lc is specified in PC units. On the
dsPIC33C/E/F device, the PC increments by 2 for each instruction word. Odd values are not
permitted. On a dsPIC33A device, the PC increments by 4 for each instruction word.
Note: A location counter is not an absolute address but the
offset from the start of the section in which the
.org occurs.The bytes between the current location counter and the new location
counter are filled with fill.
new-lc is an absolute expression. You cannot
.org backwards. You cannot use .org to cross
sections.
The new location counter is relative to the current module and is not an absolute address.
fill is optional. If not specified:
- In a data section, a value of
0x00is used to fill the skipped bytes. - In a code section, the last specified
.fillvalueis used to fill the lower two bytes of program memory and the last specified.fillupperis used to fill the upper program memory byte.