11.6.3 Run-Time Library Support
In order to initialize variables in data memory, the data initialization
template must be processed at start-up, before the application's main function takes
control. For C programs, this task is performed by C start-up modules in the runtime
library. Assembly language programs can also use the C start-up modules by linking with
libc99-pic30-elf.a.
Multiple versions of the start-up modules are contained within the runtime library. The linker will select a startup module based on commands in the linker script. For example:
CRT0_STARTUP(crt0_standard.o)
CRT1_STARTUP(crt1_standard.o)For each device, two start-up modules are specified: a primary module (CRT0) and an alternate module (CRT1).
To utilize a start-up module, the application must allow the run-time library to take control at device Reset. This happens automatically for C programs. The application’s main() function is invoked after the start-up module has completed its work. Assembly language programs should use the following naming conventions to specify which routine takes control at device Reset.
| Main Entry Name | Description |
|---|---|
__reset | Takes control immediately after device Reset |
_main | Takes control after the start-up module completes its work |
Note that the first entry name (__reset)
includes two leading underscore characters. The second entry name (_main) includes only one leading underscore character. The linker scripts
construct a GOTO __reset instruction at location 0 in program memory, which transfers control
upon device Reset.
The primary start-up module is linked by default and performs the following:
- The stack pointer (W15) and stack pointer limit register (SPLIM) are initialized, using values provided by the linker or a custom linker script. For more information, see Stack Allocation.
- If a
.constsection is defined, it is mapped into the PSV window by initializing the PSVPAG and CORCON registers. On devices which support EDS the DSRPAG register will be initialized. Note that a.constsection is defined when the “Constants in code space” option is selected in MPLAB X IDE, or the-mconst-in-codeoption is specified on the compiler command line. - The data initialization template in section
.dinitis read, causing all uninitialized sections to be cleared, and all initialized sections to be initialized with values read from program memory. - If the application has defined
user_initfunctions, section.user_initis called. - The function
mainis called with no parameters. - If
mainreturns, the processor will reset.The alternate start-up module is linked when the
--no-data-init optionis specified. It performs the same operations, except for step (3), which is omitted. The alternate start-up module is much smaller than the primary module, and can be selected to conserve program memory if data initialization is not required.Source code for both modules is provided in the
srcdirectory of the MPLAB XC-DSC C Compiler installation directory. The start-up modules may be modified if necessary. For example, if an application requiresmainto be called with parameters, a conditional assembly directive may be switched to provide this support.