10.5 Linker Script Command Language
Linker scripts are text files that contain a series of commands. Each command is either a keyword (possibly followed by arguments) or an assignment to a symbol. Multiple commands may be separated using semicolons. White space is generally ignored.
Strings such as file or format names can normally be entered directly. If the file name contains a character, such as a comma, which would otherwise serve to separate file names, the file name may be specified in double quotes. There is no way to use a double quote character in a file name.
Comments may be included just as in C, delimited by /* and */. As in C, comments are syntactically equivalent to white space.