4.5.5 Using Executable Symbols in a Data Context
The DSC device modified-Harvard
architecture includes separate address spaces for data storage and program
storage. Most instructions and assembler directives imply a context which is
compatible with symbols from one address space or the other. For example, the
CALL instruction implies an executable
context, so the assembler reports an error if a program tries to CALL a symbol located in a data section.
Likewise, instructions and directives that imply a data context cannot be used with symbols located in an executable section. Assembling the following code sequence will result in an error, as shown:
.text
msg: .asciz "Here is an important message"
mov #msg,w0
:
:
Assembler messages:
Error: Cannot reference executable symbol (msg) in a data context
In this example the mov instruction
implies a data context. Because symbol msg is
located in an executable section, an error is reported. The programmer was
possibly trying to derive a pointer for use with the PSV window. The special
operators described in Special Operators can be used whenever an executable symbol must be referenced
in a data context:
.text
msg: .asciz "Here is an important message"
mov #psvoffset(msg),w0
Here the psvoffset() operator derives a 16-bit value which is suitable for use in a data context.
The next example shows how the special symbol “.” can be used with a data directive in an executable section:
.text
fred: .long paddr(.)
Here the paddr() operator derives a 24-bit value which is suitable for use in a data context. The .long directive pads the value to 32 bits and encodes it into the .text section.