11.11.1 Gaps Between Variables of Different Types
Gaps may be inserted between variables of different types to satisfy address alignment requirements. For example, the following sequence of C statements will result in a gap:
char c1;
int i;
char c2;
int j;
Because the processor requires integers to be aligned on a 16-bit
address boundary, a padding byte was inserted after variables c1 and c2. To eliminate this padding,
variables of the same type should be defined together, as shown:
char c1,c2;
int i,j;
Gaps between variables are not visible to the linker and are not reported in the link map. To detect these gaps, an assembly listing file must be created. The following procedure can be used:
- If the source file is written in C,
specify the
-save-tempscommand line option to the compiler. This will cause an assembly version of the source file to be saved infilename.s.xc-dsc-gcc test.c -save-temps - Specify the
-ailisting option to the assembler. This will cause a table of section information to be generated.
xc-dsc-as test.s
-ai
SECTION INFORMATION:
Section Length (PC units) Length (bytes) (dec)
------- ----------------- --------------------
.text 0 0 (0)
TOTAL PROGRAM MEMORY USED (bytes): 0 (0)
Section Alignment Gaps Length (bytes) (dec)
------- -------------- --------------------
.data 0 0 (0)
.bss 0 0 (0)
.nbss 0x2 0x8 (8)
TOTAL DATA MEMORY USED (bytes): 0x8 (8)
In this example, 2 bytes of unused memory were inserted into section
.nbss. Gaps between ordinary C variables will not
exceed 1 byte per variable.