2.4.6 Configure at91bootstrap to Load a Custom Bare Metal Application from an SD Card
In this section, we will customize at91bootstrap to load and execute a Harmony3 bare-metal application directly from an SD card or e.MMC instead of U-Boot. By default, at91bootstrap is configured to load U-Boot as the second-stage bootloader, but in this scenario, we will modify sam9x60_curiositysd_uboot_defconfig or sam9x60_curiositysd1_uboot_defconfig to load the custom bare-metal application. This requires adjustments to the next software type and image storage setup to ensure that at91bootstrap correctly loads the Harmony3 bare-metal application from the storage media.
To configure at91bootstrap to load a Harmony3-based application from SD card memory into external volatile memory (DDRAM), proceed as follows:
- Go to Project→ Properties→
Kconfig→ Load→ Harmony3→ at91bootstrap→ configs→
sam9x60_curiositysd_uboot_defconfig or
sam9x60_curiositysd1_uboot_defconfig→ Open.
Figure 2-7. Load at91bootstrap SD Card Boot Configuration or
- Perform the following changes:
- SD Card Host Controller: Select SDHC0 or SDHC1, based on which card interface is used.
- Next Software Type: Load 4 MB into the start of the DDRAM.
- Demo Application Image
Storage Setup:
- External DDRAM Address to Load Demo-App Image: This should match the bare-metal application entry point address or the code section start address as specified in the linker script file.
- Next Software Image File Name: Name of the user application binary file. For this application note, use harmony.bin.
- Click Apply, then OK.
This completes the at91bootstrap configuration for loading a bare-metal application from an SD card.
An example configuration for the SAM9X60-Curiosity board is shown below.