2.4.5 Configure at91bootstrap to Load a Custom Bare-Metal Application from NAND Flash Memory
In this section, we will customize at91bootstrap to load and execute a custom bare-metal application directly from NAND Flash memory instead of U-Boot. By default, at91bootstrap is configured to load U-Boot as the second-stage bootloader, but in this scenario, we will modify the sam9x60_curiositynf_uboot_defconfig to load the bare-metal application, i.e., Harmony3. This requires adjustments to the next software type and image storage setup to ensure that at91bootstrap correctly loads the Harmony3 bare-metal application stored in NAND Flash memory.
To configure at91bootstrap to load a Harmony3 bare-metal application from NAND Flash memory into external volatile memory (DDRAM), proceed as follows:
- Go to Project→ Properties→ Kconfig→ Load→ Harmony3→ at91bootstrap→ configs→ sam9x60_curiositynf_uboot_defconfig→ Open.
- Perform the following changes:
- Next Software Type: Load 4 MB into the start of DDRAM (see Figure 2-6).
- Demo Application Image
Storage Setup:
- Flash Offset for Demo-App: NAND Flash offset where the bare-metal application is programmed. In this example, an offset of 0x40000 is chosen.
- Demo-App Image Size: Size of the image that at91bootstrap will copy from NAND to DDRAM. In this example, a demo app image size of 0xc0000 is chosen. This is taken as a safety value. It is not necessary to enter the exact application size, but rather a larger value to accommodate the different application sizes during development.
- External RAM Address to Load Demo-App Image: This should match the entry point address for the bare-metal application. This can also be verified by looking at the code section memory placement in the application linker file.
- Click Apply, then OK.
This completes the at91bootstrap configuration for loading a bare-metal application from NAND Flash memory.
An example configuration for the SAM9X60-Curiosity board is shown below.