31.3.2.4.2 ADC Voltage Reference
The reference voltage for the ADC (VREF) controls the conversion range of the ADC. Input voltages that exceed the selected VREF will be converted to the maximum result value of the ADC, for an ideal 10-bit ADC this is 0x3FF. VREF can be selected by writing the Reference Selection bits (REFSEL) in the Control C register (ADC.CTRLC) as either VDD or an internal reference from the VREF peripheral. VDD is connected to the ADC through a passive switch.
The internal reference is generated from an internal bandgap reference through an internal amplifier, and is controlled by the Voltage Reference (VREF) peripheral.