1.1.1 ADC Conversion
When using the ADCRC as the clock source for ADCC, there is a delay of one
instruction cycle between setting the ADGO bit and being able to read it as set.
This delay may result in a false conversion complete scenario (i.e., ADGO being
cleared), particularly if the user code has a bit clear test BTFSC
instruction on the ADGO bit immediately after setting it. See code example
below.
BSF ADCON0, ADGO ; Start conversion
BTSFC ADCON0, ADGO ; Is conversion done?
GOTO $-1 ; No, test again
Work around
Add a NOP instruction after setting the ADGO bit and
before testing the bit for completion of conversion. See code example below.
BSF ADCON0, ADGO ; Start conversion
NOP
BTSFC ADCON0, ADGO ; Is conversion done?
GOTO $-1 ; No, test again
Affected Silicon Revisions
| A3 | A4 | ||||||
| X |