2.6 Default Jumper Settings

The following picture shows the default jumper settings. Jumpers in blue are in open position, jumpers in red are in closed position.

Boards are delivered in a factory configuration that may not correspond to a customer-specific use case. Before using the board, double check the jumpers settings against the view and table given below.

Figure 2-2. SAMA7G54-EK Default Jumper Settings
Table 2-5. SAMA7G54-EK Jumper Settings
JumperStateFunction
J2ClosedVDDBU current measurement
J3Open (default)RMII Ethernet interface is selected.
ClosedThe 4-microphone PDMIC interface is selected.
J22Open (default)Booting from on-board memory is permanently allowed and only disabled during SW4 pressure.
ClosedBooting from on-board memory is permanently disabled.
J25Open (default)Enables UART communication (CDC) between MPU and SAM3U.
ClosedDisables UART communication (CDC) between MPU and SAM3U.
J26Open (default)The on-board J-Link interface is enabled and used for MPU debugging.
ClosedThe on-board J-Link interface is disabled. MPU debugging is done through the JTAG connector (J27).