7.1.4 PMD Control

Name: PMDCTL
Address: 0x10

Bit 15141312111098 
 FDCAPHDCAP 
Access RORORORORORORORO 
Reset 01000000 
Bit 76543210 
 TPREFNTPEN 
Access ROROROROROROR/WR/W 
Reset 00000000 

Bit 15 – FDCAP Full Duplex Capability

This bit indicates that the LAN8679 PMD does not have the ability to operate in full duplex.
ValueDescription
0 Full duplex operation is not supported
1 Full duplex operation is supported

Bit 14 – HDCAP Half Duplex Capability

This bit indicates that the LAN8679 PMD has the ability to operate in half-duplex.
ValueDescription
0 Half-duplex operation is not supported
1 Half-duplex operation is supported

Bit 1 – TPREFN Topology Discovery Reference Node select

When the PMD is configured for topology discovery operation, this bit will select which topology discovery mode the PMD operates in. When set, the PMD will function as a topology discovery measured node. When clear, the PMD will function as a topology discovery reference node. This configures the PMD topology discovery internal scrambler for the correct operation as a measured or reference topology discovery node.
Note: This bit has no effect when the Topology Discovery Enable (TPEN) bit is clear.
ValueDescription
0 PMD operates as a topology discovery measured node
1 PMD operates as a topology discovery reference node

Bit 0 – TPEN Topology Discovery Enable

When set, the PMD operates in topology discovery mode.
ValueDescription
0 Normal operation
1 Topology discovery mode