6.1.9.22 Global Directive
The GLOBAL identifier_list
directive declares a
list of comma-separated symbols. If the symbols are defined within the current module, they
are made public. If the symbols are not defined in the current module, they are made
references to public symbols defined in external modules. Thus to use the same symbol in
two modules the GLOBAL
directive must be used at least twice: once in the
module that defines the symbol to make that symbol public and again in the module that uses
the symbol to link in with the external definition.
For example:
GLOBAL lab1,lab2,lab3