This selector allows you to indicate how Device Family Pack (DFP) management
should be performed. The Do not override selection will let
the MPLAB X IDE provide a list of DFPs that can be selected. If you would like to
use a DFP that you have manually downloaded, select User specified
location and then enter the path to the DFP in the
Custom DFP path field. You may also select
Compiler location, which will use the DFPs that ship
with the compiler rather than the IDE.
Custom DFP path
If you have selected User specified location
for the Override default device support option, enter the
path to the DFP you wish to use in this field.
C standard
This selector specifies the language standard used. See Std Option.
This field allows you to fine-tune the specifications that must be processed by
smart IO functions when the compiler is unable to determine usage information from
the formatted IO function cal. See Smart-io-format Option
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.