6.1.6.4 Accessing SFRs
The symbols for Special Function Registers (SFRs) are not automatically accessible from
assembly code. The assembly header file <xc.inc> must be included
into every module that needs access to these register definitions.
Include the header file using the assembler’s INCLUDE directive, (see
Include Directive) or use the C
preprocessor’s #include directive. If you are using the latter method,
make sure you name the assembly source file using a .S extension (upper
case), or use the -xassembler-with-cpp option when you build (see X: Specify Source Language Option).
LATA. This symbol name is also made a preprocessor macro,
defined to be a string that is the same as the register's name, allowing you to confirm
that the register exists before accessing it. For
example:#ifdef LATA // if this device has a PORTA latch register...
movf LATA,w
movwf savedState
#endifbsf or btfsc etc. For
example, bit #5 inside the PORTB register can be accessed using the symbol
RB5. For example:btfss RB5
incf countbsf BANKMASK(INTCON0),INTCON0_IPEN_POSN,c ;set the IPEN bit in the INTCON0 registerSymbols
are also not defined when the field name is a single letter, for example the carry bit in
the STATUS register is called C, but there will be no symbol with this name defined. In
some cases, there might be an alternate name provided, for example CARRY,
but the field can always be access in a manner similar to that shown in the above
example.BANKMASK() or PAGEMASK()
macros or ANDing the operand with a mask) is not necessary when using the
-Wl,--fixupoverflow option and any of the
ignore, warn, or lstwarn
arguments.The <xc.inc> header supplies a complete set of field-position
equates representing the field's bit position in its register, size (in bits), and a
bitmask that can be used to perform bitwise operations on the field. These equates have the
form REGISTERNAME_FIELDNAME_SUFFIX, where
SUFFIX can be POSITION or its
alias POSN, SIZE or its alias LENGTH, or
MASK. For example, the following are defined for the RA3 field in the
PORTA register:PORTA_RA3_POSN and PORTA_RA3_POSITION,
PORTA_RA3_SIZE and PORTA_RA3_LENGTH, and
PORTA_RA3_MASK.