5.15.1 Compiler-Generated Psects
The code generator places code and data into psects, or sections, with
standard names, which are subsequently positioned by the default linker options. The linker
does not treat these compiler-generated psects any differently to a psect that has been
defined by yourself. A psect can be created in assembly code by using the
PSECT assembler directive (see Psect Directive).
The names of psects are case sensitive. Some psects use special naming
conventions, for example, the bss psect, which holds uninitialized
objects. There may be uninitialized objects that will need to be located in bank 0 data
memory; others may need to be located in bank 1 memory. As these two groups of objects will
need to be placed into different memory banks, they will need to be in separate psects so
they can be independently controlled by the linker.
The general form of data psect names is:
[bit]psectBaseNameCLASS[div]
where psectBaseName is the base name of the psect
(listed in Data Space Psects). The
CLASS is a name derived from the linker class (see Data Memory Classes) in which the psect
will be linked, e.g., BANK0. The prefix bit is used if the psect holds
__bit variables. So there can be psects like: bssBANK0, bssBANK1 and
bitbssBANK0 defined by the compiler to hold the uninitialized variables.
Note that __eeprom-qualified variables can define psects
called bssEEDATA or dataEEDATA, for example, in the same
way. Any psect using the class suffix EEDATA is placed in the HEX file and
is burnt into the EEPROM space when you program the device.
If a data psect needs to be split around a reserved area,
it will use the letters l and h (as
div in the above form) in the psect name to indicate if it is
the lower or higher division. Thus you might see bssBANK0l and
bssBANK0h psects if a split took place.
If you are unsure which psect holds an object or code in your project, check the assembly list file (see General Format).