3.3.1.1 When Should I Cast Expressions?
Expressions can be explicitly cast using the cast operator -- a type in
round brackets, e.g., (int). In all cases, conversion of one type to
another must be done with caution and only when absolutely necessary.
Consider the example:
unsigned long l;
unsigned int i;
i = l;
Here, a long type is being assigned to an int type and
the assignment will truncate the value in l. The compiler will automatically perform a type
conversion from the type of the expression on the right of the assignment operator
(long) to the type of the value on the left of the operator
(int).This is called an implicit type conversion. The compiler
typically produces a warning concerning the potential loss of data by the truncation.
A cast to type int is not required and should not be used
in the above example if a long to int conversion was
intended. The compiler knows the types of both operands and performs the conversion
accordingly. If you did use a cast, there is the potential for mistakes if the code is
later changed. For example, if you had:
i = (int)l;
the code works the same way; but if in the future, the type of
i is changed to a long, for example, then you must
remember to adjust the cast, or remove it, otherwise the contents of l
will continue to be truncated by the assignment, which cannot be correct. Most importantly,
the warning issued by the compiler will not be produced if the cast is in place.
Only use a cast in situations where the types used by the compiler are not the types that you require. For example, consider the result of a division assigned to a floating point variable:
int i, j;
float fl;
fl = i/j;
In this case, integer division is performed, then the rounded integer
result is converted to a float format. So if i contained 7 and
j contained 2, the division yields 3 and this is implicitly converted
to a float type (3.0) and then assigned to fl. If you
wanted the division to be performed in a float format, then a cast is necessary:
fl = (float)i/j;
(Casting either i or j forces the
compiler to encode a floating-point division.) The result assigned to fl
now is 3.5.
An explicit cast can suppress warnings that might otherwise have been produced. This can also be the source of many problems. The more warnings the compiler produces, the better chance you have of finding potential bugs in your code.