6.4.1 Addressing Registers from Header Files
To address registers in the supplied C header files, the following rules apply:
- A register is identified by <peripheral_instance_name>.<register_name>, e.g., CPU.SREG, USART2.CTRLA, or PORTB.DIR.
- The peripheral name is given in the “Peripheral Address Map” in the “Peripherals and Architecture” section.
- <peripheral_instance_name> is obtained by substituting any n or x in the peripheral name with the correct instance identifier.
- When assigning a predefined value to a
peripheral register, the value is constructed following the rule:
<peripheral_name>_<bit_field_name>_<bit_field_value>_gc
<peripheral_name> is <peripheral_instance_name>, but remove any instance identifier.
<bit_field_value> can be found in the “Name” column in the tables in the Register Description sections describing the bit fields of the peripheral registers.
Register Assignments
// EVSYS channel 0 is driven by TCB3 OVF event EVSYS.CHANNEL0 = EVSYS_CHANNEL0_TCB3_OVF_gc; // USART0 RXMODE uses Double Transmission Speed USART0.CTRLB = USART_RXMODE_CLK2X_gc;
Note: For peripherals with different register
sets in different modes, <peripheral_instance_name> and
<peripheral_name> must be followed by a mode name.