3.2.1 Overview
The main user interface offered by the kit is the touch user interface consisting of the:
-
6x button sensors interfaced through the TWI interface of the Atmel AT32UC3C0512C and a QVGA LCD display interfaced through the EBI interface of the AT32UC3C0512C with touch screen interfaced through the ADCIFA interface of the AT32UC3C0512C
-
4x general purpose LEDs (labeled LED0, LED1, LED2, and LED3) connected to the AT32UC3C0512C
-
The 2x push-button labeled PB0 and PB1 used as general purpose push-button
-
The push-buttons labeled RST used to generate an external reset to the AT32UC3C0512C
-
An audio jack header is connected to one channel of the DACIFB IP of the AT32UC3C0512C
-
A microphone and a potentiometer each connected to one channel of the ADCIFA interface of the AT32UC3C0512C
Note that there are other user interface components in the kit, these are related to:
-
The USB Interface is presented in USB Interface
-
The Virtual Com Port Interface is presented in USB Interface