5 Building and Running the Application
Follow these steps to program the Software Attack Protection Application on the PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit.
- Set the tz_pic32cm_ls00_cnano
project as the main project by right-clicking the project and selecting Set as
Main Project.
Figure 5-1. Make the Non-Secure Project as Main Project
- The PIC32CM LS00 Curiosity Nano+
Touch Evaluation Kit supports debugging using a Nano Embedded Debugger (nEDBG).
Connect the Type-A male to micro-B USB cable to the micro-B USB port
on the PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit to power and debug the
PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit.
Figure 5-2. PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit Hardware Setup - Go to the Project Properties, and select the Hardware Tool and Compiler:
- In the MPLAB X IDE Project Properties window perform these actions.
- Under the left Categories section, select Conf: [default], and in the
right Configuration properties sheet, select the Connected Hardware Tool and
Compiler Toolchain.
Figure 5-3. Project Properties - PIC32CM LS00 Curiosity Nano+Touch Evaluation Kit
- Click Apply, and then click OK.
- Build the project by clicking on the
Clean and Build icon or selecting Clean and Build Main Project
from the drop-down item list and verify that the project builds successfully.
Figure 5-4. Clean and Build
- Program the application by clicking the highlighted icon below.
Figure 5-5. Program the Device