4.2 Adding the Secure Application Logic
To develop and run the application, follow these steps:
- Declare the following variables and macros used by the secure application in the
main.cfile.#include <string.h> #include "non_secure_app_image_pic32cm_ls00_cnano.h" #define APP_IMAGE_SIZE sizeof(image_pattern) #define APP_IMAGE_END_ADDR (APP_IMAGE_START_ADDR + APP_IMAGE_SIZE) #define NON_SECURE_APP_ADDR (TZ_START_NS) static uint8_t *appStart = (uint8_t *)NON_SECURE_APP_ADDR; static uint8_t *dataStart = (uint8_t *)NVMCTRL_DATAFLASH_START_ADDRESS; uint8_t firmware_digest_0[64]; uint8_t firmware_digest_1[32];Figure 4-7. Declaration of Variables and Macros
- Add the Boot ROM APIs in the
main.cfile to access them as follows.typedef struct { /* Digest result of SHA256 */ uint32_t digest[8]; /* Length of the message */ uint64_t length; /* Holds the size of the remaining part of data */ uint32_t remain_size; /* Buffer of remaining part of data (512 bits data block) */ uint8_t remain_ram[64]; /* RAM buffer of 256 bytes used by crya_sha_process */ uint32_t process_buf[64]; } SHA256_CTX; SHA256_CTX sha256_ctx; typedef void (*crya_sha256_init_t) (SHA256_CTX *context); typedef void (*crya_sha256_update_t) (SHA256_CTX *context, const unsigned char *data, size_t length); typedef void (*crya_sha256_final_t) (SHA256_CTX *context, unsigned char output[32]); #define crya_sha256_init ((crya_sha256_init_t) (0x02006810 | 0x1)) #define crya_sha256_update ((crya_sha256_update_t) (0x02006814 | 0x1)) #define crya_sha256_final ((crya_sha256_final_t) (0x02006818 | 0x1)) - Include the flash_write API in the
main.cfile to program the Non-Secure firmware in the Non-Secure Flash region and write the firmware digest in the Secure Data Flash.static void flash_write(uint32_t addr, uint8_t *buf, uint32_t size) { uint32_t end_addr = addr + size; if((addr & NVMCTRL_DATAFLASH_START_ADDRESS) == NVMCTRL_DATAFLASH_START_ADDRESS) { /* Unlock the Secure Data Flash region */ NVMCTRL_RegionUnlock(NVMCTRL_SECURE_MEMORY_REGION_DATA); while(NVMCTRL_IsBusy()); } else { /* Unlock the Non-Secure Flash region */ NVMCTRL_RegionUnlock(NVMCTRL_MEMORY_REGION_APPLICATION); while(NVMCTRL_IsBusy()); } do { if(addr % NVMCTRL_FLASH_ROWSIZE == 0) { /* Erase the row */ NVMCTRL_RowErase(addr); while(NVMCTRL_IsBusy()); } /* Program 64 byte page */ NVMCTRL_PageWrite((uint32_t *)(buf), addr); while(NVMCTRL_IsBusy()); addr += NVMCTRL_FLASH_PAGESIZE; buf += NVMCTRL_FLASH_PAGESIZE; }while (addr < end_addr); } - Add the SHA-256 Hash and Non-Secure
firmware verification API to the
main.cfile for calculating the Non-Secure firmware digest.static void sha256_hash(SHA256_CTX *ctx, const uint8_t *message, uint32_t length, unsigned char digest[32]) { uint8_t dataBuf[64]; uint32_t bufIdx = 0; crya_sha256_init(ctx); do { memcpy(dataBuf, &message[bufIdx], 64); crya_sha256_update(ctx, dataBuf, sizeof(dataBuf)); bufIdx += 64; }while (bufIdx < APP_IMAGE_SIZE); crya_sha256_final(ctx, digest); }static bool non_secure_app_verify(void) { sha256_hash(&sha256_ctx, appStart, APP_IMAGE_SIZE, firmware_digest_1); if(memcmp(dataStart, firmware_digest_1, 32) != 0) { printf("Firmware is Corrupted....!"); printf("\n\r\n\r"); printf("Firmware Digest after tamper detection:"); printf("\n\r\n\r"); for(int i=0; i<32; i++) { printf("0x%X ", dataStart[i]); if((i%8 == 0) && (i != 0)) { printf("\n\r"); } } flash_write(TZ_START_NS, (uint8_t *)&image_pattern, sizeof(image_pattern)); sha256_hash(&sha256_ctx, image_pattern, APP_IMAGE_SIZE, firmware_digest_1); printf("\n\r\n\r"); printf("Restored Firmware Digest:"); printf("\n\r\n\r"); for(int i=0; i<32; i++) { printf("0x%X ", firmware_digest_1[i]); if((i%8 == 0) && (i != 0)) { printf("\n\r"); } } printf("\n\r\n\r"); printf("Genuine Firmware is restored"); } else { return false; } return true; } - Include the RTC Callback in the
main.cfor the tamper interrupt and 30-second timeout.void timeout_handler(RTC_TIMER32_INT_MASK intCause, uintptr_t context) { if(RTC_TIMER32_INT_MASK_CMP0 == (RTC_TIMER32_INT_MASK_CMP0 & intCause )) { if(non_secure_app_verify() == true) { SYSTICK_DelayMs(2000); NVIC_SystemReset(); } } if (RTC_TIMER32_INT_MASK_TAMPER == (intCause & RTC_TIMER32_INT_MASK_TAMPER)) { RTC_REGS->MODE2.RTC_TAMPID = RTC_TAMPID_Msk; printf("Software Attack Detected"); printf("\n\r\n\r"); } } - Add the following code snippets after
the SYS_Initialize API in the
main.c.sha256_hash(&sha256_ctx, image_pattern, APP_IMAGE_SIZE, firmware_digest_0); flash_write(NVMCTRL_DATAFLASH_START_ADDRESS, firmware_digest_0, sizeof(firmware_digest_0));Note:sha256_hash: Calculates the digest of the Non-Secure Firmware.flash_write: Stores the firmware digest in the Secure Data Flash region.
SYSTICK_TimerStart(); RTC_Timer32CallbackRegister(timeout_handler,0); RTC_Timer32Start(); printf("\n\r---------------------------------------------------------"); printf("\n\r Software Attack Protection Demo "); printf("\n\r---------------------------------------------------------\n\r"); if(non_secure_app_verify() != true) { printf("\n\rFirmware is Genuine"); printf("\n\r\n\r"); }Note:non_secure_app_verify: Verify the Non-Secure firmware and program the genuine copy in the Non-Secure Flash region if the verification fails.