4.3.5.1 Structure and Union Qualifiers
The compiler supports the use of type qualifiers on structures. When a
qualifier is applied to a structure, all of its members will inherit this qualification.
In the following example the structure is qualified const.
const struct {
int number;
int *ptr;
} record = { 0x55, &i };
In this case, each structure member will be read-only. Remember that all
members should be initialized if a structure is const, as they cannot
be initialized at runtime.