4.3.5.2 Bit-fields In Structures
MPLAB XC8 C Compiler fully supports bit-fields in structures.
Bit-fields are always allocated within 8-bit
words, even though it is usual to use an int type in the definition. The
first bit defined will be the LSb of the word in which it will be stored. When a bit-field is
declared, it is allocated within the current 8-bit unit if it will fit; otherwise, a new byte
is allocated within the structure.
Bit-fields can span the boundary between
8-bit allocation units; however, the code to access bit-fields that do so is extremely
inefficient. A plain bit-field is unsigned; however the -fsigned-bitfields
option can be used to change that behavior.
Consider the following definition:
struct {
unsigned lo : 1;
unsigned dummy : 6;
unsigned hi : 1;
} foo;
This will produce a structure occupying 1 byte.
If foo was ultimately linked at address 0x10, the field lo
will be bit 0 of address 0x10 and field hi will be bit 7 of address 0x10. The
LSb of dummy will be bit 1 of address 0x10.
char type or a char structure member,
instead. Be aware that some SFRs are defined as bit-fields. Most are single bits,
but some can be multi-bit objects.Unnamed bit-fields can be declared to pad out unused space between active
bits in control registers. For example, if dummy is never
referenced, the structure above could have been declared as:
struct {
unsigned lo : 1;
unsigned : 6;
unsigned hi : 1;
} foo;
A structure with bit-fields can be initialized by supplying a comma-separated list of initial values for each field. For example:
struct {
unsigned lo : 1;
unsigned mid : 6;
unsigned hi : 1;
} foo = {1, 8, 0};
Structures with unnamed bit-fields can be initialized. No initial value should be supplied for the unnamed members, for example:
struct {
unsigned lo : 1;
unsigned : 6;
unsigned hi : 1;
} foo = {1, 0};
will initialize the members lo and hi
correctly.
A bit-field that has a size of 0 is a special case. The Standard indicates that no further bit-field is to be packed into the allocation unit in which the previous bit-field, if any, was placed.