3.6.2.9 Help

The --help option displays information on the xc8-cc compiler options, then the driver will terminate.

The displayed help might differ for different device families, which can be indicated using the -mcpu option.

The --help=warning option can be used to display a list of options relating to warning suppression.

Note that options displayed by the --help command that are not documented in this compiler user's guide might not supported. See the MPLAB® XC Compiler Functional Safety Manual for options approved for use in functional safety applications.

For example:
xc8-cc -mcpu=atmega48pb --help
Usage: avr-gcc [options] file...
Options:
  -pass-exit-codes         Exit with highest error code from a phase
  --help                   Display this information
  --target-help            Display target specific command line options
  --help={common|optimizers|params|target|warnings|[^]{joined|separate|undocumented}}[,...]
                           Display specific types of command line options
  (Use '-v --help' to display command line options of sub-processes)
  --version                Display compiler version information
  -dumpspecs               Display all of the built in spec strings
  -dumpversion             Display the version of the compiler
  -dumpmachine             Display the compiler's target processor
  -print-search-dirs       Display the directories in the compiler's search path
  -print-libgcc-file-name  Display the name of the compiler's companion library
  -print-file-name=<lib>   Display the full path to library <lib>
  -print-prog-name=<prog>  Display the full path to compiler component <prog>
  -print-multiarch         Display the target's normalized GNU triplet, used as
                           a component in the library path