4.3.9.3 Flashn Qualifiers
Using both the __flashn and
const qualifiers, where n can range
from 1 thru 5, indicates that the object should be located in a different program memory
section. For correct program operation, these sections must be positioned into the correct
flash segment using the project’s linker script. Subject to your target device having the
flash segments implemented, the __flash1 qualifier is associated with
flash segment 1, which should be located in the flash segment from address 64 KB to 128 KB,
with __flash2 qualified objects placed in a section that is linked to the
segment from 128 KB to 196 KB, etc. Clearly, not all the
__flashn qualifiers will available with all
devices.
For those devices that do not have memory-mapped flash, data is read using
the RAMPZ register and the elpm instruction, allowing the full program
memory to be read.
Pointers that use these qualifiers can reference program memory, see Data Pointers.