4.3.9.1 Memx Address Space Qualifier
Using both the __memx and const
qualifiers indicates that the object is to be placed in the program space. This method
of placing objects in flash is now largely redundant, as you can perform the same task
using just the const qualifier, see Const Type Qualifier. The
__memx qualifier is not needed when compiling for any device that
maps the program memory into their data memory space, such as the avrxmega3 and tinyAVR
devices.
Pointers that use this qualifier can reference both data and program
memory spaces in a similar way to pointers to const, see Pointers to Both Memory Spaces.