9.11.3 Aligned Variable Attribute
The aligned (n) attribute instructs the
compiler to align the variable on the next n byte
boundary.
The aligned attribute can also be used on a structure member.
Such a member will be aligned to the indicated boundary within the
structure.
If the alignment value n is omitted, the
alignment of the variable is set 8 (the largest alignment value for a basic
data type).
Note that the aligned attribute is used to increase the
alignment of a variable, not reduce it. To decrease the alignment value of a
variable, use the packed attribute.