9.11.1 Address Variable Attribute
The address(addr) attribute
specifies an absolute virtual address for the variable. This attribute can
be used in conjunction with a section attribute.
address attribute can be used to start a group of variables
at a specific
address: int foo __attribute__((section("mysection"),address(0xA0001000)));
int bar __attribute__((section("mysection")));
int baz __attribute__((section("mysection")));Keep in mind that the compiler performs no error checking on the specified address. The section will be located at the specified address regardless of the memory-region ranges listed in the linker script or the actual ranges on the target device. This application code is responsible for ensuring that the address is valid for the target device and application.
Also, be aware that variables attributed with an absolute address are not accessed via GP-relative addressing. This means that they may be more expensive to access than non-address attributed variables.
Sections used to hold objects placed at an absolute address will use a name
.address.N.decl,
where N is the address and
decl is the name of the
declaration.
In addition, to make effective use of absolute sections and the best-fit
allocator, standard program-memory and data-memory sections should not be
mapped in the linker script. The built-in linker script does not map most
standard sections such as the .text,
.data, .bss, or .ramfunc
section. By not mapping these sections in the linker script, we allow these
sections to be allocated using the best-fit allocator rather than the
sequential allocator. Sections that are unmapped in the linker script can
flow around absolute sections whereas sections that are linker-script mapped
are grouped together and allocated sequentially, potentially causing
conflicts with absolute sections.
Finally, note that “small” data and bss (.sdata,
.sbss, etc.) sections are still mapped in the
built-in default linker script. This is because “small” data variables must
be grouped together so that they are within range of the more efficient
GP-relative addressing mode. To avoid conflict with these linker-script
mapped sections, choose high addresses for your absolute-address
variables.
space(prog) or
space(data), respectively. Also, see the
description for the attribute space.