6.7.7.19 Fat-lto-objects Option
The -ffat-lto-objects option requests that the compiler
generate fat object files, which contain both object code and
GIMPLE (one of GCC’s internal representations), written to
unique ELF sections. Such objects files are useful for library
code that could be linked with projects that do and do not use
the standard link-time optimizer, controlled by the
-flto option.
The -fno-fat-lto-objects form of this option, which is
the default if no option is specified, suppresses the inclusion
of the object code into object files, resulting in faster
builds. However, such object files must always be linked using
the standard link-time optimizer.