2.7.2.1 External Antennas

The WINCS02/UE/UC Modules have a small surface mount U.FL connector for an external antenna connection. The choice of antenna is limited to the antenna types that the module is tested and approved for regulatory certification.

The WINCS02/UE/UC Modules are approved to use with the antennas listed in the following table. It is permissible to use a different antenna, provided it is the same antenna type, has the same antenna gain (equal or less than) and similar in-band and out-of-band characteristics are present (refer to antenna specification sheet for cutoff frequencies).

If other antenna types are used, the OEM installer must conduct the necessary assessments and authorize the antenna with the respective regulatory agencies and ensure compliance.

Table 2-5. Approved External Antenna List with Antenna Gain for WINCS02 Module
Antenna No.Part NumberManufacturerAntenna Gain (dBi)Antenna TypeRegulatory Certification
FCC(2)(3)/ISED(2)(3)/CE/NCC/KCC/MIC/ANATEL(6)
1WXE2400 TE Connectivity/Laird External Antennas3Dipolex
2ANT-2.4-CW-RCL-RPSTE Connectivity/Linx Technologies2.3Dipolex
3RFA-02-C2M2-D034 Alead2Dipolex
4RFA-02-L2H1Aristotle2Dipolex
5RFA-02-C2H1-D034Alead2Dipolex
6RFA-02-D3Aristotle2Dipolex
7RFDPA870920IMLB301Walsin1.84Dipolex
8RFDPA870920IMAB302(5)Walsin1.82Dipolex
9RFDPA870920IMAB305Walsin1.82Dipolex
10RFDPA870910IMAB308(5)Walsin2Dipolex
11RFA-02-C2M2Aristotle2Dipolex
12RN-SMA-S-RP(5)Microchip0.56Dipolex
13W1049B030(5)Pulse2Dipolex
14RN-SMA4-RPMicrochip2.2Dipolex
Note:
  1. ‘x’ denotes the antennas covered under the certification.
  2. If the end product using the module is designed to have an antenna port that is accessible to the end user, a unique (non-standard) antenna connector (as permissible by FCC) must be used (for example, RP (Reverse Polarity)-SMA socket).
  3. If an RF coaxial cable is used between the module RF output and the enclosure, a unique (non-standard) antenna connector must be used in the enclosure wall to interface with the antenna.
  4. Contact the antenna vendor for detailed antenna specifications to review the suitability to the end product operating environment and to identify alternatives.
  5. If any of these antennas are used, an additional post-calibration step is required on the customer's application board. For more details, refer to the WINCS02 Module External Antenna Calibration Guide (DS50003753).
  6. It is strongly recommend for customers to use an antenna from the list. If a new antenna of different type or higher gain is chosen for use, the customer needs to confirm their end product's regulatory compliance with a certification lab and accept any unknown risk.