2.9.1.1 CryptoAuthPublicDataElement Object
This object defines the location and contents of a public data element in CryptoAuthentication secure elements.
{ "zone": "data", "slot": 14, "offset": 0, "data": BASE64URL(data) }
- zone
- CryptoAuthentication zone where the data are found. The options are “data” for one of the slots, “otp” for the OTP zone or “config” for the configuration zone.
- slot
- If the zone is “data”, this is the slot index (0-15) where the data can be found.
- offset
- Byte offset into the zone/slot that the data can be found at.
- data
- Actual data at the location specified by the other members. This data will be BASE64URL encoded (with padding characters (“=”) stripped).