32.3.3.6.1 Analog Input Circuit

The figure below illustrates the analog input circuit. An analog source connected to an analog input (AINn) is subject to the pin capacitance and input leakage of that pin (represented by IH and IL). When the input is selected, the source must also drive the Sample-Hold capacitor (CIN) through the combined resistance of the input path (represented by RIN). Refer to the Electrical Characteristics section for details on the ADC input characteristics.

Figure 32-2. Analog Input Schematic

If a source with high impedance is used, the sampling time may need to be increased. The required sample time depends on how long the source needs to charge the CIN capacitor and can be configured using the Sample Duration (SAMPDUR) bit field in the Control E (ADCn.CTRLE) register.

At low supply voltages, the resistance of the analog input path may increase. This raises the RC time constant of the sampling network and may require a higher SAMPDUR value to allow CIN to fully charge.