11.9.1 Packed Example
__pack_upper_byte char message[] = "Hello World!\n";
will allocate the message string into Flash memory in such a way that the upper byte of memory contains valid data.
There are no restrictions to the types of
__pack_upper_byte data. The compiler will 'pack' structures as if
__attribute__((packed)) had also been specified. This further
eliminates wasted space due to padding.
Like other extended type qualifiers, the
__pack_upper_byte type qualifier enforces a unique addressing space on
the compiler; therefore, it is important to maintain this qualifier when passing values as
parameters. Do not be tempted to cast away the __pack_upper_byte qualifier
– it won't work.