11.9.2 Usage Considerations
When using this qualifier, consider the following:
- The following attributes are not compatible with
__pack_upper_byte:bootnearreversedmanoloadxmemoryeedatapsv, auto_psvymemory __pack_upper_bytedata is best used for large data sets that do not need to be accessed frequently or that do not have important access timing.- Sequential accesses to
__pack_upper_bytedata objects will improve access performance. - A version of
mempcyis defined inlibpic30.h, and its prototype is:void _memcpy_packed(void *dst, __pack_upper_byte void *src, unsigned int len); - The following style of declaration is invalid for packed memory:
Here,__pack_upper_byte char *message = "Hello World!\n";messageis a pointer to__pack_upper_bytespace, but the string"Hello World!\n", is in normal const data space, which is not compatible with__pack_upper_byte. There is no standard C way to specify a different source address space for the literal string. Instead declaremessageas an object (such as an array declaration in 11.9.1 Packed Example). - The TBLPAG SFR may be corrupted during access of a packed variable.