24.3.14 Bit-Fields Straddling a Storage Unit Boundary
The standard indicates that implementations can determine whether bit-fields cross a storage unit boundary. In the CCI, bit-fields do not straddle a storage unit boundary; a new storage unit is allocated to the structure, and padding bits fill the gap.
Note that the size of a storage unit differs with each compiler and target device, as
this is based on the size of the base data type (for example, int) from
which the bit-field type is derived. For MPLAB XC8, this unit is 8-bits in size; for
MPLAB XC16, it is 16 bits; and for MPLAB XC32, it is 32 bits in size. For MPLAB XC-DSC
compiler, the size depends on the device used.
Example
The following shows a structure containing bit-fields being defined.
struct {
unsigned first : 6;
unsigned second : 6;
} order;
Under the CCI and using MPLAB XC8, the storage allocation unit is byte sized. The
bit-field second is allocated a new storage unit since there are only 2
bits remaining in the first storage unit in which first is allocated.
The size of this structure, order, is 2 bytes.
Differences
This allocation is identical with that used by all previous compilers.
Migration to the CCI
No action required.