6.7.4.1.16 -Wsequence-point
Warn about code that may have undefined semantics because of violations of sequence point rules in the C/C++ standard.
The C/C++ standard defines the order in which expressions in a C/C++ program are evaluated in
terms of sequence points, which represent a partial ordering between the execution of
parts of the program: those executed before the sequence point and those executed after
it. These occur after the evaluation of a full expression (one which is not part of a
larger expression), after the evaluation of the first operand of a
&&, ||, ? : or
, (comma) operator, before a function is called (but after the
evaluation of its arguments and the expression denoting the called function), and in
certain other places. Other than as expressed by the sequence point rules, the order of
evaluation of subexpressions of an expression is not specified. All these rules describe
only a partial order rather than a total order, since, for example, if two functions are
called within one expression with no sequence point between them, the order in which the
functions are called is not specified. However, the standards committee has ruled that
function calls do not overlap.
It is not specified, when between sequence points modifications to the values of objects take effect. Programs whose behavior depends on this have undefined behavior; the C/C++ standard specifies that “Between the previous and next sequence point, an object shall have its stored value modified, at most once, by the evaluation of an expression. Furthermore, the prior value shall be read only to determine the value to be stored.” If a program breaks these rules, the results on any particular implementation are entirely unpredictable.
Examples of code with undefined behavior are a = a++;, a[n] =
b[n++] and a[i++] = i;. Some more complicated cases are
not diagnosed by this option and it may give an occasional false positive result, but in
general it has been found fairly effective at detecting this sort of problem in
programs.