6.7.7.1 -Aquestion (answer)

Assert the answer answer for question question, in case it is tested with a preprocessing conditional such as #if #question(answer). -A- disables the standard assertions that normally describe the target machine.

For example, the function prototype for main might be declared as follows:

#if #environ(freestanding)
int main(void);
#else
int main(int argc, char *argv[]);
#endif

A -A command-line option could then be used to select between the two prototypes. For example, to select the first of the two, the following command-line option could be used:

-Aenviron(freestanding)