24.7 Pragmas
Pragmas may be used by a compiler to control code generation. Any compiler will ignore an unknown pragma, but many pragmas implemented by another compiler have also been implemented by the MPLAB XC16, MPLAB XC-DSC and MPLAB XC32 C compilers in compatibility mode. The table below shows the pragmas and the level of support when using each of these MPLAB XC C compilers.
Many of these pragmas take arguments. Even if a pragma is supported by an MPLAB XC C compiler, this support may not apply to all of the pragma’s arguments. This is indicated in the following table.
| IAR Compatibility Mode | |||
|---|---|---|---|
| Pragma | XC16 | XC-DSC | XC32 |
bitfields | ignore | ignore | ignore |
data_alignment | support | support | support |
diag_default | ignore | ignore | ignore |
diag_error | ignore | ignore | ignore |
diag_remark | ignore | ignore | ignore |
diag_suppress | ignore | ignore | ignore |
diag_warning | ignore | ignore | ignore |
include_alias | ignore | ignore | ignore |
inline | support (no args) | support (no args) | support (no args) |
language | ignore | ignore | ignore |
location | support | support | support |
message | native support | native support | native support |
object_attribute | ignore | ignore | ignore |
optimize | native support | native support | native support |
pack | native support | native support | native support |
__printf_args | support | support | support |
required | support | support | support |
rtmodel | ignore | ignore | ignore |
__scanf__args | support | support | support |
section | support | support | support |
segment | support | support | support |
swi_number | ignore | ignore | ignore |
type_attribute | ignore | ignore | ignore |
weak | native support | native support | native support |