4.5.9 How Big Can C Variables Be?
This question specifically relates to the size of individual C objects, such as arrays or structures. The total size of all variables is another matter.
To answer this question you need to know the memory space in which the
variable is to be located. When using the -mconst-in-code option, objects
qualified const will be located in program memory, other objects will be
placed in data memory. Program memory object sizes are discussed in the following section
of this user’s guide:
11.3.5 Size Limitations of Program Memory Variables [DD]
Objects in data memory are broadly grouped into “autos” and “non-autos.” These objects have size limitations. For more on auto and non-auto variables and the size limitations, see the following sections of this user’s guide:
11.2 Variables In Data Space Memory
11.2.3 Auto Variable Allocation and Access, "Auto Variable Size Limits"
11.2.2 Non-Auto Variable Allocation and Access, "Non-Auto Varible Size Limits"