BLE_HOGPS_SetKeyboardInputReport
C
uint16_t BLE_HOGPS_SetKeyboardInputReport(uint8_t *p_keyCodeArray);
Description
Sets HID keyboard input report.
Note
This function prepares the input report for a keyboard device in the Human Interface Device (HID) profile. The report includes modifier keys, reserved byte, and up to six keycodes representing the keys that are pressed.
Parameters
Parameter | Description |
---|---|
[in] p_keyCodeArray | An array of 8 bytes representing the keyboard report. The array is structured as follows:- Byte 0: Modifier keys (e.g., Shift, Ctrl)- Byte 1: Reserved (typically 0x00)- Bytes 2 to 7: Keycodes 1 to 6, indicating keys that are currently pressed |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | The input report was successfully set. |
MBA_RES_INVALID_PARA | The input parameters are invalid. |