BLE_HOGPS_SetBootMouseInputReport
C
uint16_t BLE_HOGPS_SetBootMouseInputReport(uint8_t buttons, int8_t xAxis, int8_t yAxis);
Description
Sets the HID boot mode mouse input report.
Note
This function prepares the input report for a mouse in HID boot mode with the current state of mouse buttons and position.
Parameters
Parameter | Description |
---|---|
[in] buttons | Bitmask representing the state of the mouse buttons:- Bit 0: Left button (1 if pressed, 0 if not)- Bit 1: Right button (1 if pressed, 0 if not)- Bit 2: Middle button (1 if pressed, 0 if not) |
[in] xAxis | The displacement of the mouse along the X-axis since the last report, in units. |
[in] yAxis | The displacement of the mouse along the Y-axis since the last report, in units. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | The input report was successfully set. |
MBA_RES_INVALID_PARA | The parameters provided are invalid. |